AXIS#.SAFEPARAM.SCA_#.POSUPPERLIMIT

Description

Indicates the absolute position upper limit of the Safe CAm (SCA) safety function.

 

Parameters Editor with the Position Upper Limit value circled

 

This is s_UL_SCA in the following diagram:

Context

For complete SCA information refer to SCA (Safe Cam).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[-2^31+1, 2^31-1]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SCA_1.POSUPPERLIMIT

316fh

02h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SCA_2.POSUPPERLIMIT

3170h

02h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SCA_3.POSUPPERLIMIT

3171h

02h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SCA_1.POSUPPERLIMIT

326fh

02h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SCA_2.POSUPPERLIMIT

3270h

02h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SCA_3.POSUPPERLIMIT

3271h

02h

Signed32

-

-

Read/Write

No